Nexans Launches New Tray Cable Range For Dynamic Applications
- Suitable for the US and Canadian markets, new automation cable range combines the advantages of a tray cable with the high performance capability of a servo motor or multicore cable designed for dynamic applications.
- Tray cables are ideally suited for a variety of applications including drag trains or moving components in automation systems as well as wind turbines.
Paris La Défense, November 28, 2017 – Tray cables have developed an excellent reputation for providing robust and reliable power and control connections for static automation applications on assembly lines, bottle filling, packaging machines or machine tools. However, the fast-moving automation sector now often calls for cables that can handle motion in several axes, severe acceleration and braking and a vast number of bending cycles. In most cases a standard tray cable wouldn’t cope. Nexans has responded by carrying out a major research and development program to create the new INTERCOND® Tray Cable range that combines the virtues of a tray cable with the dynamic capabilities of an advanced automation cable suitable for servo motor installations.
Tray Cables from the INTERCOND range are available in servo motor and multicore versions. They are suitable for dynamic applications, for example in drag chain or moving machine parts as well as in wind turbines. They offer a faster homologation process for machine tools in particular with reduced installation cost and effort as the cables can be installed without the need for metal conduits. Comprehensive testing by Nexans’ dedicated automation facility has shown that the cables provide superior dynamic performance, with up to 3 million cycles when bending at 7.5 times the cable diameter in drag chain applications as well as supporting speeds up to 240 m/min with an acceleration up to 10 m/s2.
The new tray cables are UL and CSA listed – a key requirement for machine tool makers that operate in the US and Canadian markets. They are also MTW (machine tool wires) and WTTC (wind turbine tray cable) approved. Thanks to CIC (Control and Instrumentation cable) and TC-ER (Tray Cable – Exposed Run) approvals, they can be installed without the use of metal conduits. Resistant to abrasion, as well as oils, coolants and chemicals, they are also suitable for direct burial underground without the need for any extra protection in the form of sheathing or piping. The cables can operate in temperatures varying between -5°C up to +80°C with a nominal voltage up to 1000 V.
The INTERCOND® Tray Cables are manufactured in Nexans’ Pioltello plant in Italy.
“As the automation technology evolves, Nexans looks to support the rapid change with this new range of ever-more performant tray cables for fast-moving applications”, said Bob de Kruijf, General Manager for Industry Solutions & Projects Europe. “These new dynamic tray cables will also help Nexans’ customers to be more competitive in the US and Canada where the automation market is growing fast and is becoming increasingly attractive to machine tool manufacturers, both in Europe and worldwide.”
Informacje, katalogi, broszury
Twój kontakt
About Nexans
As a global leader in advanced cabling and connectivity solutions, Nexans brings energy to life through an extensive range of best-in-class products and innovative services. For over 120 years, innovation has been the company’s hallmark, enabling Nexans to drive a safer, smarter and more efficient future together with its customers. Today, the Nexans Group is committed to facilitating energy transition and supporting the exponential growth of data by empowering its customers in four main business areas: Building & Territories (including utilities, smart grids, emobility), High Voltage & Projects (covering offshore wind farms, submarine interconnections, land high voltage), Telecom & Data (covering data transmission, telecom networks, hyperscale data centers, LAN), and Industry & Solutions (including renewables, transportation, Oil & Gas, automation, and others). Corporate Social Responsibility is a guiding principle of Nexans’ business activities and internal practices. In 2013 Nexans became the first cable provider to create a Foundation supporting sustainable initiatives bringing access to energy to disadvantaged communities worldwide. The Group’s commitment to developing ethical, sustainable and high-quality cables drives its active involvement within several leading industry associations, including Europacable, The National Electrical Manufacturers Association (NEMA), International Cablemakers Federation (ICF) or CIGRE to mention a few. Nexans employs more than 26,000 people with industrial footprint in 34 countries and commercial activities worldwide. In 2017, the Group generated 6.4 billion euros in sales. Nexans is listed on Euronext Paris, compartment A. For more information, please consult: www.nexans.com