Dynamic umbilicals for Remotely Operated Vehicles (ROVs)

  • Oil&Gas Dynamic Umbilical ROVsNexans provides cost-effective and field-proven umbilical solutions using steel or aramide armor for ROVs operating down to 7,000 meters.

  

Our customised underwater telecommunication cables are manufactured at our production facility in Rognan, on the coast of northern Norway. The modern plant has a 35 year long history of building specialised telecom cables. The plant has an excellent infrastructure such as a deep water harbour, road and rail connections.

 

Nexans provided the steel-armored umbilicals for the ROV that worked on the “Prestige” wreck off the Spanish coast, and supplied an aramid-armored cable used for oceanographic research at 7,000-meter depth in the Indian Ocean.

Files (attachements)