Nexans wins major Order for Shanghai Transrapid Project

Paris, July 16, 2001 - Nexans has been awarded an order from ThyssenKrupp Transrapid GmbH for the supply and installation of the motor winding (longstator winding) for the Transrapid track to be set up in Shanghai.

The motor winding, installed along the total length of the track belongs to the key components in the system of magnetic levitation technology, providing non-contact driving power for the planned operating speed of 420 km/h and a maximum speed of up to 500 km/h.

For the 30 km Transrapid track, a rubber-insulated 20 kV cable for stator winding with a total length of approximately 1,000 km is used. This cable is converted into a three-phase motor winding on the track and installed. In Shanghai, the product, as well as the highly automated laying technique the project requires, will be used in a large-scale project for the first time. Nexans has years of experience in this field. The Transrapid test line, built in the 1980s in Emsland/Germany, had nearly completely been equipped with a linear motor winding system from Nexans.

In addition to manufacturing the components, Nexans� specialists will support the system installation to be carried out by the Chinese customer in cooperation with ThyssenKrupp.

Deliveries for the project will start in July this year and will continue in 2002. The equipment will be produced at Nexans� Mönchengladbach (Germany) site.
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
Formed from Alcatel Cables and Components, Nexans is a worldwide leader in the cable industry. Nexans product portfolio includes an extensive range of cables and systems. Nexans solutions can be found in every area of people's lives, from telecommunications and energy networks, to aeronautics aerospace, automobile, building, petrochemical and medical applications. Operating in 20 countries, Nexans employs 19,000 people and had sales in 2000 of euros 4.8 billion. More information on www.nexans.com