Nexans wins subsea electrical heating cable contract from Statoil for the Kristin field (Norway)

Kristin Field NorwayParis, July 31, 2003 - Nexans has won a Euros 15 million contract from Statoil to supply electrical heating cables, heating cable risers and protective equipment for the subsea flowlines on the Kristin field in the Norwegian Sea.

The contract has been placed by the operator, Statoil, on behalf of the licensees for this Norwegian Sea field. It covers heating cables, electrical risers and a mechanical-protection solution for installation piggyback on the flowlines which connect the subsea installations with the floating production platform on the Kristin field. The heating system will prevent hydrate (hydrocarbon ice) from forming in the pipelines during unplanned production shutdowns.

This is the third direct electrical heating system Statoil has ordered, indicating that the system is successful and something that the company wants to focus on in future,� said Yvon Raak, Nexans� Executive Vice President, Europe Area.

The electrical heating system, which is installed on the Åsgard field in the Norwegian Sea and the Huldra field in the North Sea, has been developed by Statoil in collaboration with Nexans and other Norwegian suppliers. The wellstream of the Kristin Field has a particularly high temperature which has required further development of the piggy-back system.

The equipment will be manufactured at Nexans� Halden factory, south of Oslo, with installation work being carried out under an existing contract awarded to Technip Offshore Norge.

The Kristin field is due to produce from 12 subsea wells tied back to a floating platform. Its production capacity will be an estimated 126,000 barrels of condensate and 18 million cubic metres of gas per day. Production is planned to start in the summer of 2005.
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
Nexans is the worldwide leader in the cable industry. The Group brings an extensive range of advanced copper and optical fiber cable solutions to the infrastructure, industry and building markets. Nexans cables and cabling systems can be found in every area of people's lives, from telecommunications and energy networks, to aeronautics, aerospace, automobile, railways, building, petrochemical, medical applications, etc. The program is completed by superconducting materials and components, cryoflex transfer systems and special machinery for the cable industry. With an industrial presence in 28 countries and commercial activities in 65 countries, Nexans employs 17,150 people and had sales in 2002 of euros 4.3 billion. Nexans is listed on the Paris stock exchange. More information on http://www.nexans.com