DONG chooses Nexans subsea cable to link Hornsea Project One offshore wind farm

Order for 139 km of three-phase 34 kV subsea cable for the array cabling of the first construction phase of the 1.2 gigawatt wind farm

Paris, December 14, 2016 – Danish company DONG Energy Wind Power A/S has contracted Nexans to supply and terminate a total of 139 km of three-phase subsea cable for the first of three construction phases of the Hornsea Project One wind farm, located off the Yorkshire coast. The 34 kV cables of latest generation will be used for inter-linking a total of 58 wind turbines and connecting them to the offshore transformer station. This first stage of the wind farm, on which construction began in January, is expected to be operational within approximately three years and to produce 406 MW (1.2 GW for all three construction stages). The supply and termination of the Nexans cable will begin in spring 2018 and should be completed around a year later.

Particular features of the wind farm, which will be erected at a depth of 20 to 40 metres, are its size and distance from the coast, in addition to its output. It will be the largest offshore windfarm in the world, capable of meeting the annual electricity needs of well over one million homes and the farm is approximately 120 km from the English coast. For the first time in such a project, the teams from Nexans will be accommodated on board a supply vessel in the vicinity of the project and work in an adapted shift rotation so that they do not have to cover the large distance every day.

DONG has already used cable supplied by Nexans for several other offshore wind farms. Subsea cables from the Nexans plant in Hanover are already in operation at the Anholt wind farm (Denmark), West of Duddon Sands and Westermost Rough (Great Britain) and many more. The long-term business relationship was consolidated in autumn 2014 with the signing of a new framework agreement for offshore array cabling. The supply of cable and accessories, as well as installation, for Hornsea Project One is a call-off from that framework agreement. In addition, the teams from Nexans will install the internal cabling of all three transformer stations for Hornsea Project One in their building yards.

 

plan

The 1.2 GW Hornsea Project One wind farm will take up an area roughly as large as that of Cologne and will produce approximately enough energy to power well over one million homes. (Image source: DONG)

cable

The 34 kV medium-voltage cable for the Hornsea Project One wind farm contains optical fibres for communication alongside three energy cables. (Image source: Nexans)

 

Informacje uzupełniające
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
As a global leader in advanced cabling and connectivity solutions, Nexans brings energy to life through an extensive range of best-in-class products and innovative services. For over 120 years, innovation has been the company’s hallmark, enabling Nexans to drive a safer, smarter and more efficient future together with its customers. Today, the Nexans Group is committed to facilitating energy transition and supporting the exponential growth of data by empowering its customers in four main business areas: Building & Territories (including utilities, smart grids, e­mobility), High Voltage & Projects (covering offshore wind farms, submarine interconnections, land high voltage), Telecom & Data (covering data transmission, telecom networks, hyperscale data centers, LAN), and Industry & Solutions (including renewables, transportation, Oil & Gas, automation, and others). Corporate Social Responsibility is a guiding principle of Nexans’ business activities and internal practices. In 2013 Nexans became the first cable provider to create a Foundation supporting sustainable initiatives bringing access to energy to disadvantaged communities worldwide. The Group’s commitment to developing ethical, sustainable and high-quality cables drives its active involvement within several leading industry associations, including Europacable, The National Electrical Manufacturers Association (NEMA), International Cablemakers Federation (ICF) or CIGRE to mention a few. Nexans employs more than 26,000 people with industrial footprint in 34 countries and commercial activities worldwide. In 2017, the Group generated 6.4 billion euros in sales. Nexans is listed on Euronext Paris, compartment A. For more information, please consult: www.nexans.com

About DONG Energy

DONG Energy is one of the leading energy groups in Northern Europe. Our business is based on procuring, producing, distributing and trading in energy and related products. Headquartered in Denmark, DONG Energy has around 6,500 employees, including over 600 in the UK. The Group generated DKK 67 billion (EUR 9.0 billion) in revenue in 2014. For further information, see www.dongenergy.co.uk.