New EDRMAX by Nexans™ cable ensures faster and easier grid connections for renewables

Nexans has developed a new medium voltage cable suitable for installation in any type of ground conditions to provide cost effective utility grid connections.

Paris, October 12, 2016 – Nexans, in collaboration with the utility managing the majority of France’s public electricity distribution network, has developed and tested a new generation of medium voltage (MV) cables for the connection of power sources to the grid. Known as EDRMAX by Nexans, the new cable is eco-designed for a reduced environmental impact. It allows easier installation compared to the previous EDR version, particularly in challenging conditions like hard or rocky ground.

New EDRMAX by Nexans™ cable ensures faster and easier grid connections for renewablesThe EDRMAX by Nexans solution has been designed specifically to enable the grid connection of renewable energy resources such as solar panels or wind turbines. This development is an illustration of Nexans’ contribution to address the growing demand for energy across the world. EDRMAX by Nexans™ is compliant with the NFC 33-226 standard. It is available in single or three-core versions, with either aluminium or copper conductor. EDRMAX™ allows a maximum permissible current in permanent service above 400 A and has a Class 2 (C2) rating for flame non-propagation performance.

A key advantage of the EDRMAX by Nexans design is the high mechanical strength provided by its oversheathing that enables the cable to be buried directly into the ground with no need for an additional sand layer. Furthermore, the flexibility of the cable makes it easy to handle and this combined with its high stripability with standard tools provides a faster connected cable solution.

Nexans technical teams have co-designed this new cable to meet one of the environmental impact reduction targets. It is one of the first cables to comply with Nexans’ new Eco-design approach that takes account of the entire product life cycle spanning manufacture, use and end-of-life. An additional benefit of EDRMAX by Nexans™ is that the joule losses have been reduced significantly compared with the existing EDR and this contributes to a 12%[1] lower impact on global warming across the whole cable life cycle from sourcing of raw materials to recycling.

Nexans is manufacturing the EDRMAX by Nexans™ cable at its facility in Bourg en Bresse, France.

Yvan Duperray, VP for European Utilities Sales at Nexans said, “The development of EDRMAX by Nexans™ illustrates how we aim to go above and beyond when it comes to meeting the technical challenges set by our customers. With our innovations on this product, we were able to find a solution that not only makes the grid connection of renewables faster, easier and more cost-effective, it also offers a more environmentally friendly solution.”

 

[1] The result is given for one kilometer of EDR 3x240 sq. mm aluminum conductor cable with a life span of 40 years, an average usage scenario (1/4 time at 25, 50, 75 and 100% of max. intensity where max. intensity is 466A), and considering the French energy mix. The result is computed from the life cycle analysis performed in accordance with the 14040-44 standard.

The life cycle stages taken into account are manufacture, transportation, installation, use and end-of-life. For the 13 environmental indicators assessed, the impact reductions are similar to those observed for climate change.

Informacje uzupełniające
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
As a global leader in advanced cabling and connectivity solutions, Nexans brings energy to life through an extensive range of best-in-class products and innovative services. For over 120 years, innovation has been the company’s hallmark, enabling Nexans to drive a safer, smarter and more efficient future together with its customers. Today, the Nexans Group is committed to facilitating energy transition and supporting the exponential growth of data by empowering its customers in four main business areas: Building & Territories (including utilities, smart grids, e­mobility), High Voltage & Projects (covering offshore wind farms, submarine interconnections, land high voltage), Telecom & Data (covering data transmission, telecom networks, hyperscale data centers, LAN), and Industry & Solutions (including renewables, transportation, Oil & Gas, automation, and others). Corporate Social Responsibility is a guiding principle of Nexans’ business activities and internal practices. In 2013 Nexans became the first cable provider to create a Foundation supporting sustainable initiatives bringing access to energy to disadvantaged communities worldwide. The Group’s commitment to developing ethical, sustainable and high-quality cables drives its active involvement within several leading industry associations, including Europacable, The National Electrical Manufacturers Association (NEMA), International Cablemakers Federation (ICF) or CIGRE to mention a few. Nexans employs more than 26,000 people with industrial footprint in 34 countries and commercial activities worldwide. In 2017, the Group generated 6.4 billion euros in sales. Nexans is listed on Euronext Paris, compartment A. For more information, please consult: www.nexans.com