Meyer Werft cruise liners equipped with Nexans SHIPLINK® cables

Paris, July 27, 2015 – The Anthem of the Seas, a luxury cruise liners built at the Meyer Werft shipyard in Germany, set sail with Nexans cables on board. The Norwegian Escape, another new luxury cruise ship currently under construction at Meyer Werft, will also be equipped with Nexans cables. Supplying Nexans cable range for these two vessels is part of a multi-year contract which represents the continuation of a 25 year partnership between the two companies.

Meyer Werft cruise liners equipped with Nexans SHIPLINK® cablesNexans supplies low voltage power cables, instrumentation and control cables and medium voltage power cables, essential for the operation of the cruise liners. Around 3,000 km of cables have been delivered for Anthem of the Seas and some 2,400 km will be supplied for Norwegian Escape.

The cables are halogen-free, fire retardant and exhibit special performances in respect of smoke emission and toxic gases under fire conditions. Nexans developed a new fire resistance standard to meet the demands of the project. The cables are designed to last for the lifetime of the ship which is expected to be around 25 years. The cables will be manufactured at Nexans’ plant in Monchengladbach, Germany, a dedicated global shipbuilding cable factory.

Meyer Werft cruise liners equipped with Nexans SHIPLINK® cablesRoyal Caribbean’s Anthem of the Seas is the world’s third largest cruise ship with a capacity of more than 4,000 passengers over 18 decks. Norwegian Cruise Line’s Norwegian Escape has a capacity of 4,200 passengers and is expected to be delivered later this year.

Sven Smid, Lead purchase manager for cables at Meyer Werft said, “We have had a fruitful relationship with Nexans in the past and are looking forward to that continuing it in the future. Nexans understands Meyer Werft and the needs of our projects.”

“Nexans has a long standing relationship with Meyer Werft to whom we have delivered thousands of kilometres of cables during the last 25 years we have worked together. This contract further connects Nexans and Meyer Werft and we are delighted of this successful collaboration,” added Stephane Mortelette, Shipbuilding Segment Manager at Nexans.

Informacje uzupełniające
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
Nexans brings energy to life through an extensive range of cables and cabling solutions that deliver increased performance for our customers worldwide. Nexans’ teams are committed to a partnership approach that supports customers in four main business areas: Power transmission and distribution (submarine and land), Energy resources (Oil & Gas, Mining and Renewables), Transportation (Road, Rail, Air, Sea) and Building (Commercial, Residential and Data Centers). Nexans’ strategy is founded on continuous innovation in products, solutions and services, employee development, customer training and the introduction of safe, low-environmental-impact industrial processes.
In 2013, Nexans became the first cable player to create a Foundation to introduce sustained initiatives for access to energy for disadvantaged communities worldwide.
Nexans is an active member of Europacable, the European Association of Wire & Cable Manufacturers, and a signatory of the Europacable Industry Charter. The Charter expresses its members' commitment to the principles and objectives of developing ethical, sustainable and high-quality cables.
We have an industrial presence in 40 countries and commercial activities worldwide, employing close to 26,000 people and generating sales in 2014 of 6.4 billion euros. Nexans is listed on NYSE Euronext Paris, compartment A.
For more information, please consult: www.nexans.com

www.nexans.com