NSN Link will interconnect Nordic and British energy markets with the world’s longest subsea power link incorporating Nexans’ HVDC cable technology

Power interconnection beneath the North Sea will enable Norway and UK to share up to 1400 MW of green energy from 2021 onwards.
Statnett SF and National Grid has awarded Nexans a contract valued at around Euros 340 million to deliver the subsea cable on the Norwegian side.

Skagerrak Copyright Nexans Paris, July 14, 2015The NSN Link under the North Sea will enable a two-way exchange of green energy between the Nordic and British markets through a 730 km submarine HVDC (high voltage direct current) submarine cable system for which Nexans will design, manufacture and install the major section on the Norwegian side. The 1400 MW link, comprising two 525 kV cable systems, is due for completion in 2021. Nexans’ contract for Statnett SF and National Grid is valued at Euros 340 million.

Norway and the UK plan to generate more power from renewable sources in order to meet their domestic and international renewable and climate change targets. The NSN Link is being created in collaboration between Statnett, the state owned operator in the Norwegian energy system and the UK’s National Grid. It is designed to help increase opportunities for shared use of renewable energy.

When wind power production in the UK is high, Norway will be able to import power at a lower price than in the Nordic market, helping conserve the water in the country’s hydropower reservoirs. At times when there is little wind in the UK, then it can import Norwegian hydropower at a lower price than in the UK, while helping to ensure security of power supplies.

The NSN Link will run from Blyth in Northumberland on the north east coast of the UK to Kvilldal in Rogaland on the Norwegian side. HVDC converter stations on each side will connect the link to the onshore grid.

Nexans has been awarded the contracts for Lot 1 of the NSN Link – the Fjord submarine section and the Norwegian tunnel/lake and underground cable for the onshore connection on the Norwegian side. With two cable sub-systems, the contract covers the design, manufacture and installation of some 500 km of mass impregnated non-draining (MIND) HVDC cables at depths down to 600 metres off the coast of Norway. The cables will be laid by Nexans’ own cable-laying vessel, C/S Nexans Skagerrak and protected on the seabed by trenching with Nexans’ Capjet system and rock dumping. Nexans will also provide a shorter length of underground cable for the onshore connection.

Cable-SK4-uten-fiber Copyright NexansThe Nexans cables will feature the same reliable and well proven design implemented successfully for the Skagerrak 4 project for the 140 km subsea HVDC interconnector between Denmark and Norway and also selected for the ongoing NordLink project to connect the Norwegian and German power grids.

“Nexans is delighted to be playing a key role in the creation of the NSN Link, which will be the world’s longest subsea power interconnection.” said Dirk Steinbrink, Nexans Senior Executive Vice President High Voltage & Underwater Cables,

Arnaud Poupart-Lafarge, Nexans' Chief Executive Officer added “Following so closely on winning a major contract for the NordLink between Norway and Germany earlier in 2015, this is further confirmation of Nexans as the leader in HVDC cable technology for Europe’s developing network of subsea interconnectors. With this new order, we are very proud to have reached a cumulated order book of 2 billion Euros“.

The NSN Link cables will be developed, tested and manufactured at Nexans’ Halden plant in Norway.
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
Nexans brings energy to life through an extensive range of cables and cabling solutions that deliver increased performance for our customers worldwide. Nexans’ teams are committed to a partnership approach that supports customers in four main business areas: Power transmission and distribution (submarine and land), Energy resources (Oil & Gas, Mining and Renewables), Transportation (Road, Rail, Air, Sea) and Building (Commercial, Residential and Data Centers). Nexans’ strategy is founded on continuous innovation in products, solutions and services, employee development, customer training and the introduction of safe, low-environmental-impact industrial processes.
In 2013, Nexans became the first cable player to create a Foundation to introduce sustained initiatives for access to energy for disadvantaged communities worldwide.
Nexans is an active member of Europacable, the European Association of Wire & Cable Manufacturers, and a signatory of the Europacable Industry Charter. The Charter expresses its members' commitment to the principles and objectives of developing ethical, sustainable and high-quality cables.
We have an industrial presence in 40 countries and commercial activities worldwide, employing close to 26,000 people and generating sales in 2014 of 6.4 billion euros. Nexans is listed on NYSE Euronext Paris, compartment A.
For more information, please consult: www.nexans.com

www.nexans.com