Statnett’s Inner Oslofjord cable systems to reinforce Norwegian grid with Nexans subsea cables

Two new cable systems will reinforce the electricity grid in central Eastern Norway. Contract is valued at around Euros 50 million and will cover the design, manufacture and installation of XLPE cables

Nexans Inner Oslofjord cableParis, July 15, 2015 Statnett, the state owned transmission system operator in the Norwegian energy system, is reinforcing the country’s electricity network with the Inner Oslofjord power connection project based on Nexans subsea cable technology. In a project worth around Euro 50 million, Nexans will design and manufacture two new 420 kV subsea cable systems.

Statnett is investing in the Inner Oslofjord project to ensure security of power supplies for customers in central Eastern Norway by replacing two existing links built in 1958 and 1975. The new cable systems will also add value by enabling the exchange of power with Sweden.

The project covers two new links: One will connect Solberg in Hurum and Brenntangen in Vestby Municipality (Solberg-Brenntangen) and the other Filtvet in Hurum and Brenntangen in Vestby Municipality (Filtvet-Brenntangen). Each link will comprise seven individual cables based on Nexans state-of-the-art XLPE (cross-linked polyethylene) cable technology installed at a maximum water depth of 220 m.

Nexans will design, manufacture and test the cables for the Inner Oslofjord at its facility in Halden Norway. The cables will be laid by Nexans with Statnett’s cable-laying vessel, M/S Elektron and protected on the seabed by trenching with Nexans’ Capjet system. The project is due for completion in 2018.

Ragnhild Katteland, Technical and Project Operations in Nexans Submarine High Voltage division, said, “Winning the contract for the Inner Oslofjord project further reinforces Nexans’ long standing working relationship with Statnett. It also confirms that whatever the transmission technology, AC or DC, and whatever the cable technology, Nexans is the cable supplier of choice for subsea cable systems.”
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
Nexans brings energy to life through an extensive range of cables and cabling solutions that deliver increased performance for our customers worldwide. Nexans’ teams are committed to a partnership approach that supports customers in four main business areas: Power transmission and distribution (submarine and land), Energy resources (Oil & Gas, Mining and Renewables), Transportation (Road, Rail, Air, Sea) and Building (Commercial, Residential and Data Centers). Nexans’ strategy is founded on continuous innovation in products, solutions and services, employee development, customer training and the introduction of safe, low-environmental-impact industrial processes.
In 2013, Nexans became the first cable player to create a Foundation to introduce sustained initiatives for access to energy for disadvantaged communities worldwide.
Nexans is an active member of Europacable, the European Association of Wire & Cable Manufacturers, and a signatory of the Europacable Industry Charter. The Charter expresses its members' commitment to the principles and objectives of developing ethical, sustainable and high-quality cables.
We have an industrial presence in 40 countries and commercial activities worldwide, employing close to 26,000 people and generating sales in 2014 of 6.4 billion euros. Nexans is listed on NYSE Euronext Paris, compartment A.
For more information, please consult: www.nexans.com

www.nexans.com