Nexans wins major subsea umbilical contract from Equinor for Troll Phase 3 development

Nexans will provide a total of 27 kilometers of complex umbilicals with power, fiber-optic and hydraulic elements for the next development phase of the most prolific oil and gas field on the Norwegian continental shelf.

Paris La Défense, July 3, 2018 – The Troll oil and gas field is the most prolific field on the Norwegian continental shelf (NCS), with more than half of its reserves still remaining after over 20 years of production. The initial development was carried out over two phases, and now Equinor is starting the Phase 3 development to recover the large amount of gas resources in the western part of the field. Nexans will play a vital role in the Troll Phase 3 project by supplying Equinor with the complex umbilicals required to power and control the subsea systems.

Nexans wins major subsea umbilical contract from Equinor for Troll Phase 3 development Phase 3 of the Troll project covers the development of the Troll West structure, which lies in water depths of approximately 330 meters and is located 25 kilometers north-west of the Troll A platform. The subsea production systems will comprise two subsea templates or manifolds, as well as nine trees. Each manifold is expected to have four well slots. A total of eight production wells will be drilled and tied-back to the Troll A platform in order to recover the gas reserves. First gas is expected from the project in the second quarter of 2021.

For the Troll Phase 3 development Nexans Norway will design, manufacture and supply static umbilicals that include high voltage power elements, high-pressure hydraulic lines, low-pressure hydraulic lines, a MEG (methanol and glycol) service line for chemical injection, a spare line and fiber-optic communications – all within a single cross-section. A 20 kilometer umbilical will link the Troll A platform to Template W1, while a 7 kilometer umbilical will then link Template W1 to Template W2. The contract also includes the supply of connections, terminations and other umbilical accessories.

Nexans offered Equinor a total ‘made in Norway’ approach to the contract with the electrical and fiber optic elements manufactured at the Nexans Norway facility in Rognan, North Norway, while the complete umbilical system will be developed, manufactured and tested at Nexans Norway plant in Halden, Norway. 

Vincent Dessale, Nexans Senior Executive Vice President Subsea and Land Systems Business Group, said: “Nexans has established an impressive track record in delivering umbilical projects for the Norwegian continental shelf and we look forward to continuing our long-standing relationship with Equinor by delivering this key contract for Troll Phase 3".

Nexans is scheduled to deliver the Troll Phase 3 umbilicals in the first quarter of 2020.

Informacje, katalogi, broszury

Twój kontakt

Angéline Afanoukoe Press relations
Telefon +33 1 78 15 04 67
Angeline.afanoukoe@nexans.com
Michel Gédéon Financial Communication
Telefon +33 1 78 15 05 41
michel.gedeon@nexans.com
Ksenia Kanareva Press relations
Telefon Tel: +33 (0) 1 78 15 04 74
ksenia.kanareva@nexans.com
Marième Diop Financial Communication
Telefon +33 1 78 15 05 40
marieme.diop@nexans.com

About Nexans

As a global leader in advanced cabling and connectivity solutions, Nexans brings energy to life through an extensive range of best-in-class products and innovative services. For over 120 years, innovation has been the company’s hallmark, enabling Nexans to drive a safer, smarter and more efficient future together with its customers. Today, the Nexans Group is committed to facilitating energy transition and supporting the exponential growth of data by empowering its customers in four main business areas: Building & Territories (including utilities, smart grids, e­mobility), High Voltage & Projects (covering offshore wind farms, submarine interconnections, land high voltage), Telecom & Data (covering data transmission, telecom networks, hyperscale data centers, LAN), and Industry & Solutions (including renewables, transportation, Oil & Gas, automation, and others). Corporate Social Responsibility is a guiding principle of Nexans’ business activities and internal practices. In 2013 Nexans became the first cable provider to create a Foundation supporting sustainable initiatives bringing access to energy to disadvantaged communities worldwide. The Group’s commitment to developing ethical, sustainable and high-quality cables drives its active involvement within several leading industry associations, including Europacable, The National Electrical Manufacturers Association (NEMA), International Cablemakers Federation (ICF) or CIGRE to mention a few. Nexans employs more than 26,000 people with industrial footprint in 34 countries and commercial activities worldwide. In 2017, the Group generated 6.4 billion euros in sales. Nexans is listed on Euronext Paris, compartment A. For more information, please consult: www.nexans.com